Unsuable demo app: evkmimxrt1064_lwip_httpssrv_ota_enet MISSING MCUboot bootloader source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unsuable demo app: evkmimxrt1064_lwip_httpssrv_ota_enet MISSING MCUboot bootloader source

Jump to solution
548 Views
avbot
Contributor III

Examples:  evkmimxrt1064_lwip_httpssrv_ota_enet   AND   evkmimxrt1064_ota_demo_enet
require MCUBoot bootloader.
RT1064 has ROM bootloader, but am I understanding correctly that these demos need custom version of MCUBoot bootloader programmed into Flash to run?

Text from demo app readme:
"The demo requires MCUBoot bootloader to be present in the FLASH memory to function properly.
It is recommended to build and program the bootloader first, then go on with the application.
Please refer to respective readme of the mcuboot_opensource example "

Please provide the source for MCUBoot bootloader for RT1064 as soon as possible.

0 Kudos
1 Solution
543 Views
avbot
Contributor III

Thanks.. actually I just found it in 1064 SDK 2.12, feature needs to be configured first.

View solution in original post

2 Replies
544 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) RT1064 has ROM bootloader, but am I understanding correctly that these demos need custom version of MCUBoot bootloader programmed into Flash to run?
-- Yes.
2) You can find the demo of mcuboot_opensource resides ~\boards\evkbmimxrt1060 of SDK library.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
544 Views
avbot
Contributor III

Thanks.. actually I just found it in 1064 SDK 2.12, feature needs to be configured first.