We have a production system which programs all our production systems using a Segger JLINK tool.
We want to only use this tool and not the mfgTools, however we have found that the code is not executed unless the board has been programmed once by the mfgTools. (The same happens trying to debug a simple hello world program in MCUXpresso, if the board hasn't been programmed with the mfg tools you can't load and debug the program).
We are using external QSPI Flash as out boot device.
Is there are way to replicate what is done with the MFgTools by programming with the Segger, so that we can eliminate this step in our production process.
Thanks in advance to anybody who can help with this problem.
Solved! Go to Solution.
Hi @FillmoreSys
Please check my english document:
Chpater 2, although for RT600, you still can refer to it, similiar to the RT10XX.
Best Regards,
Kerry
Hi @FillmoreSys ,
So the issue is only happens on the new customer RT1050 board + QSPI chip.
Your mentioned issue is mainly related to the QE bit, as you know, to the QSPI chip, QE bit is the non-volatile bit, to the new chip, it need to configure the QE bit at first to enable the quad mode, then in the app, it can be read with quad mode.
Normally, this is related to the JLINK flash driver, please tell me which JLINK version you are using now?
You can try our RT-UFL flash algo, this will help to configure the QE bit.
https://github.com/JayHeng/RT-UFL/archive/refs/tags/v1.0.zip
https://www.cnblogs.com/henjay724/p/14942574.html
https://www.cnblogs.com/henjay724/p/15430619.html
Please try it.
If you still have issues about it, please kindly let me know.
Please also let me know your QSPI flash chip partnumber. As different QSPI flash has the different QE bit position.
Best Regards,
Kerry
Hi Kerry ,
The info you asked for is this
JLINK S/W = JLINK_V758C
QSPI = IS25LP128
The part is a MIMXRT1052DVL6B
The Device type I have selected in the segger is MIMXRT1052xxxxB which I have removed form the Jlink XML File.
I will give your flash loader a try later today.
Regards
David
Hi @FillmoreSys
Thanks for your information.
As I know, to the RT1050, the JLINK firmware is default for the hyperflash, as the MIMXRT1050-EVKB board is using the hyperflash, so if you want to use the QSPI flash, you need to change the firmware to the QSPI at first.
I highly suggest you try the RT-UFL, as it can support your QSPI directly with JLINK. Very easy to use.
If you don't know how to use it, just kindly let me know, as the post is in chinese.
Wish it helps you!
Best Regards,
Kerry
Hi Kerry,
If you could provide some info in English about the boot loader I would be grateful.
My Chinese is non existent.
Thanks
David
Hi @FillmoreSys
Please check my english document:
Chpater 2, although for RT600, you still can refer to it, similiar to the RT10XX.
Best Regards,
Kerry
Thanks very much for your help Kerry.
This was a great solution to my problem
David