USB VCOM Example Failure

cancel
Showing results for 
Search instead for 
Did you mean: 

USB VCOM Example Failure

Jump to solution
810 Views
jaredm
Contributor III

I'm trying to run the USB VCOM example project on RT1052-based custom hardware. My setup is as follows:

1. Import example project.

2. Remove BOARD_FLASH in linker script. The example fits in 128K internal RAM with ample margin.

3. Modify CONTROLLER_ID to be kUSB_ControllerEhci1. My hardware uses the second USB controller.

4. Compile and run the project.

I can debug the application and step through code.

I've also attached a Beagle USB analyzer. The RT1052 USB controller responds when attached to my PC, but does not ACK the initial SETUP/DATA0 request. I've attached a trace from the Beagle. You can see the ACK is missing after SETUP/DATA0. When I unplug/replug the USB cable, the RT1052 attempts to re-initialize the USB stack and the same problem occurs. (Demonstrates that the USB stack is not frozen, and the problem is repeatable.)

Does anyone have ideas as to what might be wrong?

Labels (1)
0 Kudos
1 Solution
802 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi jaredm,

Could it be a hardware problem? I test on my EVB. It works fine.

 

Regards,

Jing

View solution in original post

0 Kudos
2 Replies
803 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi jaredm,

Could it be a hardware problem? I test on my EVB. It works fine.

 

Regards,

Jing

0 Kudos
791 Views
jaredm
Contributor III

Hi Jing,

You are correct, it was a hardware problem.

On my board, I have a 5-pin header for GND, D-, D+, ID, and 5V0. Since I do not have a test fixture yet, I soldered a USB cable directly to the PCB for testing. Unfortunately, I mixed up the D- and D+ wires. After I soldered the D- and D+ wires to the correct locations, the example worked perfectly.

Thanks for the suggestion!

jaredm

0 Kudos