UART_SDP_DISABLE bit in the BOOT_PARAM4 of eFuse address 0x9A.

cancel
Showing results for 
Search instead for 
Did you mean: 

UART_SDP_DISABLE bit in the BOOT_PARAM4 of eFuse address 0x9A.

Jump to solution
593 Views
takayuki_ishii
Contributor IV

Hello community,

 

I have 2 question about eFUSE bit of IMXRT1170.

In RT1170 Reference Manual Table 26-7. Boot parameter fusemap,

BOOT_PARAM4 have 2 SDP_DISABLE bit.

Which function does it select enable/disable?

1) UART_SDP_DISABLE : BOOT_PARAM4[1]

2) SDP_DISABLE : BOOT_PARAM4[0]

 

Best regards,

Ishii.

 

Tags (1)
0 Kudos
1 Solution
586 Views
jay_heng
NXP Employee
NXP Employee

Both UART and USB port can be used as SDP interface in BootROM.

SDP_DISABLE bit - whole SDP interfaces

UART_SDP_DISABLE bit - just UART port

View solution in original post

0 Kudos
2 Replies
587 Views
jay_heng
NXP Employee
NXP Employee

Both UART and USB port can be used as SDP interface in BootROM.

SDP_DISABLE bit - whole SDP interfaces

UART_SDP_DISABLE bit - just UART port

0 Kudos
580 Views
takayuki_ishii
Contributor IV

Hello jay_heng,

 

Thank you for your quick reply.

I will answer it to my customer.

 

Best regards,

Ishii.

 

0 Kudos