Hi there,
I am trying to trigger the ADC1 on the IMX1064 via PWM1 by utilizing AD_ETC and XBAR functionality (in a similar fashion as in AN12214). I have used the config-tools -> peripherals settings to do this but I can´t seem to get the ADC_ETC to be triggered by the PWM submodule 0 counter. How would you go about to use the pinmux tool and peripheral tool to trigger the ADC1 with a PWM signal?
Best regards,
Carl
Solved! Go to Solution.
So, I got it to work when I started from a new project. If someone else needs to do this in the future, the way I did it was by creating a new project and including the relevant drivers right away:
Then, I configured (in the pinmux tool) ADC_ETC to be triggered by the flexpwm signal and also configured the pins used for the ADC and PWM like so:
After this, I set up the PWM1 submodule 0 in the peripheral tools to be triggered by VAL2 (since I will only use PWM1A for this application):
Next, the XBAR configuration for the ADC_ETC was configured like this:
And lastly, the ADC:
Also note that all peripheral use the same clock source (here IPG_CLK_ROOT - BOARD_BootClockRUN: 150 MHz).
AN12214 was of great help as well as this article https://www.programmersought.com/article/84265106737/
So, I got it to work when I started from a new project. If someone else needs to do this in the future, the way I did it was by creating a new project and including the relevant drivers right away:
Then, I configured (in the pinmux tool) ADC_ETC to be triggered by the flexpwm signal and also configured the pins used for the ADC and PWM like so:
After this, I set up the PWM1 submodule 0 in the peripheral tools to be triggered by VAL2 (since I will only use PWM1A for this application):
Next, the XBAR configuration for the ADC_ETC was configured like this:
And lastly, the ADC:
Also note that all peripheral use the same clock source (here IPG_CLK_ROOT - BOARD_BootClockRUN: 150 MHz).
AN12214 was of great help as well as this article https://www.programmersought.com/article/84265106737/