Timeout while waiting for high throughput clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Timeout while waiting for high throughput clock

Jump to solution
1,064 Views
emmmmmmmmmmmmmm
Contributor III

I have an RT1170 board. When I test the 4343W routine, the log prints 'Timeout While Waiting For High Throughput Clock', when starting the WiFi firmware, I want to know what the reason?
My WiFi model is 43438a1, I believe that my WiFi module is normal, I verify the function on the RT1052 board

0 Kudos
1 Solution
998 Views
emmmmmmmmmmmmmm
Contributor III

Thank you for your reply, I have found the reason, it is the problem of my board.

View solution in original post

0 Kudos
4 Replies
1,056 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi emmmmmmmmmmmmmm,

  Could you please tell me which detail wifi module you are using?

  From our RT1170 SDK, it has this requirement:

Hardware requirements
=====================
- 2x Micro USB cable
- MIMXRT1170-EVK board
- Personal Computer
- Murata 1DX or 1LV M.2 module
- Murata uSD M.2 Adapter
- 1 plug to receptable header cable

 

BTW, which detail SDK code you are testing?

This one:

SDK_2.9.1_MIMXRT1170-EVK\boards\evkmimxrt1170\wifi_cypress_examples\wiced_iperf_4343W

In fact, if you want to use wifi, we highly recommend you use the NXP wifi module:

SDK_2.9.1_MIMXRT1170-EVK\boards\evkmimxrt1170\wifi_examples

Hardware requirements
=====================
- Micro USB cable
- MIMXRT1170-EVK board
- Personal Computer
- One of the following WiFi modules:
- Panasonic PAN9026 SDIO ADAPTER + SD to uSD adapter
- AzureWave AW-NM191NF-uSD

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
1,050 Views
emmmmmmmmmmmmmm
Contributor III

The project I use is SDK_2.8.1_MIMXRT1170-EVK-PRC3 \ Boards \ evkmimXRT1170 \ wifi_cypress_examples \ wiced_iperf_4343w
My WiFi is NM372SM
What details do you still need?

0 Kudos
1,023 Views
kerryzhou
NXP TechSupport
NXP TechSupport

HI @emmmmmmmmmmmmmm 

  Thanks for your updated information, your SDK version is very slow, highly suggest you download the newest SDK version:

mcuxpresso.nxp.com

BTW,  please use the project related readme.txt required WIFI module, otherwise, it may still related to your own wifi module configuration. You'd better make the original wifi project works at first, then try to modify it to match your own wifi module.

 

Best Regards,

kerry

0 Kudos
999 Views
emmmmmmmmmmmmmm
Contributor III

Thank you for your reply, I have found the reason, it is the problem of my board.

0 Kudos