Throughput expected with Murata module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Throughput expected with Murata module

Jump to solution
988 Views
romitchatterjee
Contributor V

I have been working with different NXP i.MX RT boards. I am not sure what is the maximum throughput I should expect to see with the Murata modules (1DX, 1MW?, 1LV? - not sure if the last two are supported). Can someone help me with this information?

Thanks.

Labels (2)
1 Solution
861 Views
puja_sah
Contributor II

Hello Romit,

The new SDK release i.e. SDK 2.6.1 includes the support for both 1DX and 1LV. 1MW is not included but it is on the roadmap to be included in the future release. If you are able to increase the TCP window size, you should be able to see TCP throughput up to 40Mbps. All the steps to increase the TCP window size are included in our use guide. You can find it murata's website:

https://wireless.murata.com/datasheet?/RFM/data/murata_quick_start_guide_freertos.pdf

Hope it answers your question.

Thanks,

Puja

View solution in original post

3 Replies
861 Views
romitchatterjee
Contributor V

Thanks puja.sah@murata.com‌, that was very helpful!

0 Kudos
862 Views
puja_sah
Contributor II

Hello Romit,

The new SDK release i.e. SDK 2.6.1 includes the support for both 1DX and 1LV. 1MW is not included but it is on the roadmap to be included in the future release. If you are able to increase the TCP window size, you should be able to see TCP throughput up to 40Mbps. All the steps to increase the TCP window size are included in our use guide. You can find it murata's website:

https://wireless.murata.com/datasheet?/RFM/data/murata_quick_start_guide_freertos.pdf

Hope it answers your question.

Thanks,

Puja

861 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Romit Chatterjee ,

   As I know, 1DX board is tested in the SDK, 1LV module also can be supported, but 1MW  is not tested, so 1MW can't  be promised.

   I also share the related 1DX board link for your reference:

https://wireless.murata.com/usd-m2.html

https://wireless.murata.com/type-1dx.html

https://www.embeddedartists.com/products/1dx-m-2-module/

In my opinion, if you are using the RT chip, please use the 1DX or 1LV module.

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------