The i.MX rt1050 looks really nice. My question is if there is a Eagle Library available for the BGA?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The i.MX rt1050 looks really nice. My question is if there is a Eagle Library available for the BGA?

1,190 Views
thomasnielsen
Contributor II

The title says it all: Is there a Eagle library available for getting started using the i.MX rt1050?

Labels (1)
Tags (1)
0 Kudos
1 Reply

986 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Thomas,

An Eagle library is not available. However, you could refer to the “MIMXRT1050-EVK Design files” package, which includes Allegro files (schematic, layout, gerbers) at the following link:

https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...

 

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos