Support for iMXRT Series has been removed from KElL 5.24.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support for iMXRT Series has been removed from KElL 5.24.2

1,433 Views
wernerabbler
Contributor I

Keil has set the DFP 1.0.1  for the new RT1052 processor to "offline". Keil support says "that DFP is not working because of bugs, this must be fixed by NXP, then it will be available again".  Is there any information when a corrected version will be available ?

Labels (2)
Tags (3)
0 Kudos
1 Reply

1,137 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Werner,

The software team is aware of the issue, and they are working on getting the new DFP released. I just checked the MDK5 software packs page, and the new version isn't posted yet but it should be there any day now

Regards,

Carlos

0 Kudos