SVD file for MIMXRT1021?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SVD file for MIMXRT1021?

1,055件の閲覧回数
dmarples
Contributor IV

Hi there,

I think the title says it all really - is there an SVD available for this family?  The SVD for the 1050/60 is just different enough to cause troubles when you try to use it.  I don't see one in the V11 pack file or anywhere else on line, but perhaps I'm not looking in the right places....

Regards

DAVE

ラベル(1)
0 件の賞賛
2 返答(返信)

937件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the document as it https://community.nxp.com/docs/DOC-334307.Hope it help you.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

937件の閲覧回数
dmarples
Contributor IV

Thanks for this, but I was sort of hoping there might be one knocking

around. I can obviously create one using the 1050/60 as a base, but there

are subtle differences between the chips and it's easy to miss a few....

Regards

Dave

0 件の賞賛