SRC->SRSR updates with value 0x3..

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRC->SRSR updates with value 0x3..

1,151 Views
nsnmaniram
Contributor III

working with low power mode application on IMXRT1050,  i am facing issues:

1. i am able to switch from over run mode to low speed run mode without any issues.

2. while switching from low speed run to over run mode, controller gets reset:

      SRC->SRSR updates with value 0x3..

please let me know the reason for the reset.

NOTE: i am following the power switch example given in SDK 2.5.0 

this is on a customized board with IMXRT1050 chip set.

Thank you,

Maniram     

Labels (1)
0 Kudos
5 Replies

1,012 Views
jeremyzhou
NXP Employee
NXP Employee

Hi maniram nagothi,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
After testing, I find the SRC-SRSR had already been 0x03 when running the evkbimxrt1050_power_mode_switch_bm demo, so it's not caused by the modes switch.
Hope this is clear.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,012 Views
nsnmaniram
Contributor III

hi,

thank you for checking on your side and sharing the details, i want to know when this particular register will be set?

if could share the cases which can set this register, it will be more helpful.

thanks,

Maniram

0 Kudos

1,012 Views
jeremyzhou
NXP Employee
NXP Employee

Hi maniram nagothi,

Thanks for your reply.
SRC_SRSR is the indicator of reset events for the chip, so I'd like to learn the information about the 'indicator' via reviewing the RM directly.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,012 Views
nsnmaniram
Contributor III

thanks for the reply, can i know is there any way to generate the linker script for xpresso IDE, so that lpm.c variables could be saved on the SRAM location.

Thanks,

Maniram

0 Kudos

1,012 Views
jeremyzhou
NXP Employee
NXP Employee

Hi maniram nagothi.

Thanks for your reply.
To provide the fastest possible support, I'd recommend you to refer to

Placing data into different RAM blocks to view the details.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos