SRAM base address should be set as 0xA000_0000

cancel
Showing results for 
Search instead for 
Did you mean: 

SRAM base address should be set as 0xA000_0000

Jump to solution
824 Views
george
Senior Contributor II

Dear All,

Does the NOR interface behave the same as the SRAM interface with respect to “set SRAM base address as 0xA000_0000 to avoid this behavior” ?

And does it happen in 8bit data widht mode?

BR,

George

0 Kudos
1 Solution
594 Views
jay_heng
NXP Employee
NXP Employee

Hi George,

  It is not about SEMC, it is up to ARM arch, so PRAM interface should have the same limitation, and for PNOR, it doesn't support AXI write.

Best Regards,

Jay

View solution in original post

0 Kudos
3 Replies
594 Views
jay_heng
NXP Employee
NXP Employee

Hi George,

  

  What kind of NOR do you mean? Parallel NOR over SEMC or Serial NOR over FlexSPI?

pastedImage_1.png

Best Regards,

Jay

0 Kudos
594 Views
george
Senior Contributor II

Dear jayheng‌,

Thank you for your reply.

My concern is that using the parallel NOR interface via SEMC generates four bus cycles similar to the post described above.

Does this occur in either Psedo-RAM mode or Parallel NOR mode?

BR,

George

0 Kudos
595 Views
jay_heng
NXP Employee
NXP Employee

Hi George,

  It is not about SEMC, it is up to ARM arch, so PRAM interface should have the same limitation, and for PNOR, it doesn't support AXI write.

Best Regards,

Jay

0 Kudos