The reference manual "IMXRT1064RM.pdf" notes that RTC Wakeup is a possibility when in SVNS power mode (Chapter 13, Table 13-1. Low Power Mode Definition). However, the same project power_mode_switch does not allow this to occur.
There is a comment in the power_mode_switch project that says the following:
/* In SNVS mode, only SNVS domain is powered, GPT could not work. */
So, can SNVS be woken from RTC or not?
Hello
I hope you are well.
Yes, imxRT1064 can be woken up from SNVS mode through RTC. However, GPT does not work in SNVS mode, the RTC yes.
If you have more questions do not hesitate to ask me.
Best regards,
Omar