Hello,
I am trying to create my custom GUI applications with SLN-TLHMI-IOT and I can't debug and flash my work on the kit via MSD and as guides suggest I don't have a j-link. Is it possible for me to use the MCU-Link Debug tool for flashing and debugging the kit?
Thank you in advance!
Best Regards,
Gencay Akyuz
解決済! 解決策の投稿を見る。
Dear Gencay Akyuz,
Sure, this external debugger has i.MX RT1170 as one Supported Device, I just tested to build and run successfully in a SLN-TLHMI-IOT using MCU-Link as debugger.
I hope this information help you!
related case: Re: SLN-TLHMI-IOT Smart HMI Kit Flashing - NXP Community
kind regards
Ramon.
Hello Ramon,
Thank you for your answer. I am trying to build and debug the coffee machine project, it builds without a problem but when I try to debug it pops up below error. I can see the bootloader log from the terminal but nothing pops up on the display.
0 0 [BOOTLOADER_Task]
*** BOOTLOADER v1.1.0 ***
1 0 [BOOTLOADER_Task] Jumping to main application...
2 0 [BOOTLOADER_Task] [FICA] VERSION 3
3 0 [BOOTLOADER_Task] [FICA] RT Flash Check...
4 0 [BOOTLOADER_Task] [FICA] Found Flash device!
5 0 [BOOTLOADER_Task] [FICA] Checking Image Config Area (ICA) initialization
6 0 [BOOTLOADER_Task] [FICA] Flash ICA already initialized
7 0 [BOOTLOADER_Task] [FICA] Flash ICA initialization complete
8 0 [BOOTLOADER_Task] Launching into application at 0x30100000
Starting CM4 core.
I can't also flash the device via the MSD method. Again there is nothing on the display only the backlight is powered. I tried to create a blinky project by using a built-in RGB LED at the K2 pin but it does not light the LED but I can see a variable changing from the IDE and the bootloader keeps trying to load the program at 0x30100000 address again and again in a loop which I can read from the terminal.
My main goal is to see the applications that I created from GUI-Guider on SLN-TLHMI-IOT board. I am using an MCU-Link as a debugger, the SDK that I use is SDK_2.x.MIMXRT1170-EVK 2.13 my IDE is v11.7.0.
Can you suggest anything to develop on this board?
Thank you in advance!
Best Regards,
Gencay
Dear Gencay,
Could you please help me to open a new ticket to solve this new topic, sorry for the inconvenience.
kind regards.
-Ramon.
Dear Gencay Akyuz,
Sure, this external debugger has i.MX RT1170 as one Supported Device, I just tested to build and run successfully in a SLN-TLHMI-IOT using MCU-Link as debugger.
I hope this information help you!
related case: Re: SLN-TLHMI-IOT Smart HMI Kit Flashing - NXP Community
kind regards
Ramon.