SDK error: Invalid Addresses in CMSIS-SVD File for iMXRT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK error: Invalid Addresses in CMSIS-SVD File for iMXRT1170

506 Views
Masmiseim
Senior Contributor I

Hello NXP team,

 

The CMSIS-SVD files which comes with the SDKs are used in many development environments to make the peripheral registers visible in the debugger.

 

For the iMXRT1160 and iMXRT1170 family the base addresses of the following registers are invalid (set to zero) in the SVD file from SDK 2.11.0:

  • AUDIO_PLL
  • ETHERNET_PLL
  • OSC_RC_400M
  • PHY_LDO
  • TMPSNS
  • VIDEO_PLL
  • VMBANDGAP

Best regards

 

Masmiseim_0-1646586135940.png

 

0 Kudos
2 Replies

485 Views
Masmiseim
Senior Contributor I

Hello jingpan,

thanks for clarification.

It was a bit confusing having these registers listed with seemingly invalid addresses. Debugger will list them as available to watch, but they will show invalid values as they refer to the ITCM (on the M7 core).

In my opinion this is misleading.

 

Best regards

0 Kudos

491 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Masmiseim ,

Please refer to section 15.7 Analog IP interface. The analog peripherals you mentioned are all listed here. So, I think the address here is not in CM7 address range.

 

Regards,

Jing