Hello,
I'm using the MIMXRT685, I want the system clock ti be 160Mhz. I tried to change the clock configuration using MCUXpresso config tools but apparently it doesn't support this device. Can u help?
Thank u
Hello Tay,
Please try to use latest version of IDE and SDK. I used MCUXpresso IDE v11.2.1 and SDK 2.8.2 to test this and I was able to set system clock to 160 MHz using MCUXpresso Config Tools. Please check the image below.
Hope it helps!
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------