Rt1052 Compiling and running with arm-none-eabi-gcc does not work in sdrma

cancel
Showing results for 
Search instead for 
Did you mean: 

Rt1052 Compiling and running with arm-none-eabi-gcc does not work in sdrma

Jump to solution
595 Views
wandongli
Contributor I

      I migrated the project under keil to linux and compiled it with gcc. The MIMXRT1052xxxxx_flexspi_nor.ld script in sdk2.3 works fine, but it does not work with MIMXRT1052xxxxx_sdram_txt.ld.I uploaded my project, please help me to see it, after the normal download, the serial port will have output, the baud rate is 921600.

Labels (1)
0 Kudos
1 Solution
502 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi wangdong,

   Do you try the RT1050 newest SDK code sdk2.5.0?

   Which can be downloaded from this link:

  Welcome | MCUXpresso SDK Builder 

   Whether the official code works OK on your side or not?

 


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
503 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi wangdong,

   Do you try the RT1050 newest SDK code sdk2.5.0?

   Which can be downloaded from this link:

  Welcome | MCUXpresso SDK Builder 

   Whether the official code works OK on your side or not?

 


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos