Read Jedec Id using SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Read Jedec Id using SPI

1,448件の閲覧回数
adi2Intel
Contributor III

Hi all!

we are checking the implementation of NXP MX1050 to our product.

on our previous MCU we used single SPI for things like erasing and flashing external chip.

we are trying to do the same with NXP but cant find examples for this on the SDK.

 

for example - on old MCU, we connected the 5 signals : MISO, MOSI, CS, CLK, GND and send a command request with an "opcode" (0x9F) to read the Jedec ID of the external chip (returns on MISO bus)

is there an example for this kind of operation on the SDK?

 

the closest we have found is flex_component_nor but it looks like QSPI with 4 data signals and we cant  determine  the 5 single spi signals (MISO, MOSI, CS, CLK, GND) there like in the lpspi examples (on J24 arduino )

LPSI is enabled and lpspi_btb examples works

 

Adi from Intel

0 件の賞賛
3 返答(返信)

1,440件の閲覧回数
jay_heng
NXP Employee
NXP Employee

Yes, you can use both FlexSPI and LPSPI to read JEDEC id from Flash.

There is FlexSPI example in \SDK_2.11.0_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\flexspi\nor\polling_transfer, you need to update this example to enable FlexSPI 1bit SDR mode, then it will only use 2 data lines.

There is not LPSPI example, but you can refer to \SDK_2.11.0_EVKB-IMXRT1050\boards\evkbimxrt1050\bootloader_examples\flashloader. the reference code in spi_nor_eeprom_memory.c, it uses LPSPI to r/w NOR Flash.

0 件の賞賛

1,418件の閲覧回数
adi2Intel
Contributor III

Hi and thanks for the answer

Can you help us find the "1bit SDR mode" configuration?

should I replace each occurrence of "kFLEXSPI_Command_SDR" with "kFLEXSPI_Command_MODE1_SDR" ???

and after that, how do we translate these :

 

adi2levy_0-1650970375228.png

into MISO MOSI CS CLK ?

 

0 件の賞賛

1,411件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @adi2Intel ,

The LUT table is described in section 27.5.7 in reference manual. After read this section you will know how to modify it according to your design.

In Single mode, flash transmit/receive data on 1 Data pin (DATA0 for transmitting, DATA1 for receiving).

 

Regards,

Jing

0 件の賞賛