In the reference manual for i.MX RT500, an OTP Fuse Map spreadsheet is mentioned, which the manual says is attached. However, this Fuse Map doesn't actually seem to be included in the reference manual download. Is the OTP Fuse Map spreadsheet available right now for the RT500, and if so could a download link be provided?
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is the OTP Fuse Map spreadsheet available right now for the RT500, and if so could a download link be provided?
-- After checking, I think the fuse map spreadsheet hasn't been available now.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------