RT1176

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,213 Views
723809366
Contributor I

Dear NXP:

         您好,当前我们想要使用车规级1176用于开发车载应用产品,当前查看1176手册芯片满足AEC-Q100,但似乎没有明确是否可以满足功能安全的硬件需求,请问RT1176是否可以用于开发车载功能安全产品。

0 Kudos
1 Solution
1,172 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
关于你的疑惑,我会跟AE部门确认后再给你一个确切的回复。
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
1,197 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
非常感谢使用NXP产品,很高兴为你提供技术支持!
1)请问RT1176是否可以用于开发车载功能安全产品。
-- 可以的,你还有什么需要了解的吗?
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
1,186 Views
723809366
Contributor I

Hello jeremyzhou:

         感谢您的回复,我同时咨询了供应商,供应商的技术支持反馈RT1176不能使用在功能安全产品开发上,当前很是困惑。

         相比NXP S32系列,S32官网介绍页面中明确写明了ASIL与符合ISO26262,而RT1176暂无明确注明,是否是有什么其它考虑。以及若将RT1176用于开发汽车功能安全产品是否需要获取RT1176相关证明或证书?

0 Kudos
1,148 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

以下是AE 部门同事的回复:

i.MX RT1170 (Auto version) isn't an ASIL-rated device but QM. As a QM device, it only can be used in ASIL A/B system/application, cannot support ASIL D application.

Have a great day.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,173 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
关于你的疑惑,我会跟AE部门确认后再给你一个确切的回复。
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos