I am developing using imx1176.
imx1176 should receive 12bits data from FPGA.
I know that imx1176 does not support raw12 type.
So I tried to use rgb565 as 16bits.
However, I found that rgb565 is changed from mipi csi-2 to rgb888. (RGB565 -> RGB888)
What DATA TYPE should FPGA transmit to receive 12bits data.
What data type should the FPGA transmit
Hi @hdyuk,
There is no supported 12 bit RGB format, so YUV would have to be used as the alternative.
I believe this community post might prove useful for your inquiry: iMXRT1176 MIPI-CSI2 to UVC reducing the frame buffer's size.
BR,
Edwin.