RT1176 SEMC SRAM configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 SEMC SRAM configuration

933 Views
VicKrawciw
Contributor I

The following code is my setup of RT1176 SEMC for 2 x AS6C6416 8MB SRAM, one at address 0x80000000, the other 0x80800000 using ADMUX.

I only seem to be able to write reliably to the first 64 bytes of either SRAM device using a ‘memset((void*)(0x80000000), val, 8*1024*1024)’ command.

 

I cannot work out the SRAMCR0 register in the SEMC – specifically the COL bits. What does ROW/COL have to do with config of SRAM as mentioned in section 29.3.1.7.1 of the RM? The SRAM is just a linear device. The SEMC_ConfigureSRAMWithChipSelection function just sets this to 12 bits but I do not understand what this relates to.

I have setup IOCR after my call to fix the problem whereby SEMC_ConfigureSRAMWithChipSelection does not configure the CS options correctly.

 

void InitSEMC()

{

 

// ## OperationBody [d3982da8-e248-4298-ba70-fb4b1870e3a8]

  semc_config_t config;

  semc_sram_config_t sramconfig;

  uint32_t clockFrq = CLOCK_GetRootClockFreq(kCLOCK_Root_Semc);

 

  /* Initializes the MAC configure structure to zero. */

  memset(&sramconfig, 0, sizeof(semc_sram_config_t));

 

  /* Initialize SEMC. */

  SEMC_GetDefaultConfig(&config);

  SEMC_Init(SEMC, &config);

 

  /* Configure SRAM. */

  sramconfig.cePinMux = kSEMC_MUXRDY;               /*!< The CE# pin mux setting. */

  sramconfig.addr27 = kSEMC_MORA27_NONE;            /*!< The Addr bit 27 pin mux setting. */

  sramconfig.address = 0x80000000;                  /*!< The base address. */

  sramconfig.memsize_kbytes = 8 * 1024;             /*!< The memory size in unit of kbytes. 8MB*/

  sramconfig.addrPortWidth = kSEMC_PortSize16Bit;   /*!< The address port width. */

  sramconfig.advActivePolarity = kSEMC_AdvActiveLow;/*!< ADV# polarity 1: active high, 0: active low. */

  sramconfig.advLevelCtrl = kSEMC_AdvLow;           /*!< ADV# level control during address hold state, 1: low, 0: high. */

  sramconfig.addrMode = kSEMC_AddrDataMux;          /*!< Address mode. */

  sramconfig.burstLen = kSEMC_Nor_BurstLen1;        /*!< Burst length. */

  sramconfig.portSize = kSEMC_PortSize16Bit;        /*!< Port size. */

  sramconfig.syncMode = kSEMC_AsyncMode;            /*!< Sync mode. */

  sramconfig.waitEnable = false;                    /*!< Wait enable. */

  sramconfig.waitSample = 0;                        /*!< Wait sample. */

  sramconfig.tCeSetup_Ns = 0;                       /*!< The CE setup time. */

  sramconfig.tCeHold_Ns = 0;                        /*!< The CE hold time. */

  sramconfig.tCeInterval_Ns = 0;                    /*!< CE interval minimum time. */

  sramconfig.readHoldTime_Ns = 0;                   /*!< read hold time. */

  sramconfig.tAddrSetup_Ns = 20;                    /*!< The address setup time. */

  sramconfig.tAddrHold_Ns = 0;                      /*!< The address hold time. */

  sramconfig.tWeLow_Ns = 25;                        /*!< WE low time for async mode. */

  sramconfig.tWeHigh_Ns = 0;                        /*!< WE high time for async mode. */

  sramconfig.tReLow_Ns = 30;                        /*!< RE low time for async mode. */

  sramconfig.tReHigh_Ns = 0;                        /*!< RE high time for async mode. */

  sramconfig.tTurnAround_Ns = 10;                   /*!< Turnaround time for async mode. */

  sramconfig.tAddr2WriteHold_Ns = 10;               /*!< Address to write data hold time for async mode. */

  sramconfig.tWriteSetup_Ns = 0;                    /*!<Write data setup time for sync mode. */

  sramconfig.tWriteHold_Ns = 0;                     /*!<Write hold time for sync mode. */

  sramconfig.latencyCount = 1;                      /*!<Latency count for sync mode. */

  sramconfig.readCycle = 0;                         /*!<Read cycle time for sync mode. */

  sramconfig.delayChain = 0;   /*!< Delay chain, which adds delays on DQS clock to compensate timings while DQS is faster than

                         read data. */

 

  //SRAM1

  SEMC_ConfigureSRAMWithChipSelection(SEMC, kSEMC_SRAM_CS0, &sramconfig, clockFrq);

 

  //SRAM2

  sramconfig.cePinMux = kSEMC_MUXCSX0;              /*!< The CE# pin mux setting. */

  sramconfig.address = 0x80000000 + (8*1024*1024);  /*!< The base address. */

 

  SEMC_ConfigureSRAMWithChipSelection(SEMC, kSEMC_SRAM_CS1, &sramconfig, clockFrq);

 

  //Fix the driver! Set the IOCTL to correct values for RDY and CSX0 as CS0 and CS1

  SEMC->IOCR = SEMC_IOCR_MUX_CSX0(0x08) | SEMC_IOCR_MUX_RDY(0x06);

// ## OperationBody End

 

}

0 Kudos
1 Reply

894 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

The customer found that the cause of the issue was ADV# polarity, SRAM access appears to be working.

To write in SRAM you might use the SDRAM method used in the SDK example. SRAM addresses are decoded in column/row direction, this is done internally. The default value is 12 but for your specific value, I suggest you contact the memory manufacturer.
CS is not set correctly through SEMC_ConfigureSRAMWithChipSelection(). Configuring directly through the register is suggested.

It is important to check your memory details in MCUXpresso to check that non-cacheable mem is not on the SEMC_SRAM region(0x8000_0000):

Omar_Anguiano_0-1657061211826.png

 

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos