RT1170 support QSPI Flash (MX25L51245G )

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1170 support QSPI Flash (MX25L51245G )

1,199 Views
WJC
Contributor I

Hi,

Can RT1170 support MX25L51245G for QSPI flash?

Do it need to modify the configuration file “evkmimxrt1170_flexspi_nor_config.c” to meet this chip?

If so, how to modify it? Which parameters should be modified?

 

Thanks for your support!

Best regards,

WJC

0 Kudos
Reply
1 Reply

1,178 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can RT1170 support MX25L51245G for QSPI flash?
-- Yes.
2) Do it need to modify the configuration file “evkmimxrt1170_flexspi_nor_config.c” to meet this chip?
-- Yes, please refer to the below code.

const flexspi_nor_config_t qspiflash_config = {
    .memConfig =
        {
            .tag              = FLEXSPI_CFG_BLK_TAG,
            .version          = FLEXSPI_CFG_BLK_VERSION,
            .readSampleClksrc=kFlexSPIReadSampleClk_LoopbackFromDqsPad,
            .csHoldTime       = 3u,
            .csSetupTime      = 3u,
            // Enable DDR mode, Wordaddassable, Safe configuration, Differential clock
            .sflashPadType = kSerialFlash_4Pads,
            .serialClkFreq = kFlexSpiSerialClk_100MHz,
            .sflashA1Size  = 64u * 1024u * 1024u,
            .lookupTable =
                {
                    // Read LUTs
                    FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x20),
                    FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),
                },
        },
    .pageSize           = 256u,
    .sectorSize         = 4u * 1024u,
    .blockSize          = 256u * 1024u,
    .isUniformBlockSize = false,
};


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply