RT1170-EVK rev C4 schematics

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1170-EVK rev C4 schematics

ソリューションへジャンプ
1,225件の閲覧回数
mastupristi
Senior Contributor I

Hello,

downloadable from site (https://www.nxp.com/webapp/Download?colCode=MIMXRT1170-EVK-DESIGNFILES ) there is only revision C3 of the schematics SCH 32171, but I have C4. For example, I have one more switch than the schematic (SW3).

Where can I find the SCH 32171 rev C4 schematics?

 

best regards

Max

タグ(4)
0 件の賞賛
1 解決策
1,149件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, the reset button is on page 26 and is the same, for example as the RT1064.
Pavel_Hernandez_0-1681750741935.png

 

スポイラ
RT1064
Pavel_Hernandez_1-1681750780315.png

 

Let me know if you need more information.

Best regards,
Pavel

元の投稿で解決策を見る

0 件の賞賛
4 返答(返信)
1,195件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I review your information the schematic is not available at this moment, but you totally can refer to the Rev C3, as the schematic and the PCB is totally the same, just one point to the C4:

Pavel_Hernandez_0-1681510122816.png

Pavel_Hernandez_1-1681510130432.png

FXOS87OO is EOL, so rev C4 take is as DNP, others are totally the same.

Schematic just use C3.

Best regards,
Pavel

0 件の賞賛
1,165件の閲覧回数
mastupristi
Senior Contributor I

However ,I cannot find the circuit diagram related to the SW3 button.

EVK.png

 

It says in the user guide that it has to do with the POR

Screenshot_2023-04-17_08-29-34.png

But I need to know exactly how this SW3 is connected with the POR pin, such as are there pull ups or capacitors? What values?

 

best regards

0 件の賞賛
1,150件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, the reset button is on page 26 and is the same, for example as the RT1064.
Pavel_Hernandez_0-1681750741935.png

 

スポイラ
RT1064
Pavel_Hernandez_1-1681750780315.png

 

Let me know if you need more information.

Best regards,
Pavel

0 件の賞賛
1,212件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, let me get into your case and when I have more information, I will contact you.

Best regards,
Pavel

0 件の賞賛