RT1064 | issues with second stage bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1064 | issues with second stage bootloader

551 次查看
shai_b
Senior Contributor II

Hello team,

My customer has the following issue. please see the details below:

 

The bug is when I’m trying to enable write to flash using flexspi_nor_write_enable() func from flexspi_nor_flash_ops.c provided by MCUxpresso SDK.

SPI timeout configuration .AHBWriteWaitUnit     = kFLEXSPI_AhbWriteWaitUnit512AhbCycle

Still getting error kStatus_FLEXSPI_DeviceTimeout = 7002.

Could you please advise back?, Thanks in advance

KR,

Shai

 

标签 (1)
0 项奖励
1 回复

533 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the FOTA solution to implement the SD card OTA.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励