RT1064 OCRAM调整为0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1064 OCRAM调整为0

1,330 Views
colinluan
Contributor III

Hi, @jeremyzhou 

RT1064的FlexRAM可否实现OCRAM=0,DTCM=256KB, ITCM=256KB?

我在我的工程中已经实现了OCRAM=128KB,DTCM=128KB, ITCM=256KB,但是我试图实现OCRAM=0时,出现了以下问题:

colinluan_0-1618203676206.png

我的配置如下:

1、FlexRAM配置

colinluan_1-1618203774378.png

2、  ld文件配置

colinluan_2-1618203834714.png

3、MPU配置

colinluan_3-1618203890983.png

我尝试把Region7注释掉,并没有什么效果

以上的问题可能是因为什么引起的呢?RT1064是否支持配置OCRAM=0?(只能本身的512KB OCRAM)

 

 

0 Kudos
5 Replies

1,298 Views
crist_xu
NXP Employee
NXP Employee

您好,您说的没有效果是什么意思?是ocram可以访问吗

0 Kudos

1,324 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
非常感谢使用NXP产品,很高兴为你提供技术支持!
首先,对于你的问题,我的回答是可以实现的,其次,
建议参考此篇经验分享来完成FlexRAM重新配置:
https://www.nxpic.org.cn/module/forum/thread-619452-1-1.html。
跟着,在ld文件配置中,你不需要直接更改ld文件,上述经验分享会告诉你怎么修改RAM的空间配置,最后,Region7 是需要注释掉的。
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,317 Views
colinluan
Contributor III
我是在mcxpresso下开发的
0 Kudos

1,319 Views
colinluan
Contributor III
你好,链接已经失效了。 另外,我是直接使用ld文件的,并没有使用界面配置的方式,这种情况是需要改ld文件的吧?
0 Kudos

1,301 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
感谢回复,链接可以打开的。
https://www.nxpic.org.cn/module/forum/thread-619452-1-1.html
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos