RT1061,SD Card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1061,SD Card

676 Views
xupengfei1997
Contributor I

I use RT1061 to configure SD Card, SD Card is mounted successfully.

But when creating the file system, it will fail with error FR_NOT_READY.
Where the problem might be?

Labels (2)
Tags (2)
0 Kudos
1 Reply

601 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello,

 

Have you checked the examples we have available in our MCUXpresso SDK?

sdcard_fatfs example mounts a file system based on a SD card and then does "creat directory/read directory/create file/write file/read file" operation.

 

You can download the SDK in this link: https://mcuxpresso.nxp.com/en/welcome

 

Best regards,

Felipe

0 Kudos