RT1061 + 3V Octal boot flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1061 + 3V Octal boot flash

573 Views
PatrickHerron
Contributor I

Since I'm using most of the pins on the MIMXRT1061, I need to have all ports at 3.3V and not able to use 1.8V octal flash (byte mode).

Do you know any flash manufacturer that offers 3V word mode octal flash?

Can MIMXRT1061 boot and run with 3V octal flash (Marconix MX25645) with word mode(DTR-OPI) and not byte mode like all the 1.8V octal flash?

3v Octal Flash word mode (MX25645G)

PatrickHerron_1-1601670826461.png

1.8V Octal flash byte mode (MX25UM51345G)

PatrickHerron_2-1601670963884.png

Thank You.

0 Kudos
1 Reply

555 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Do you know any flash manufacturer that offers 3V word mode octal flash?
-- Macronix, Micron, Adesto, ISSI, etc.
2) In my opinion, the i.mx RT1060 can boot up from the MX25645, the i.mx RT1060 supports the Auto Probe feature which can recognize the connected Nor flash, then configure it automatically to enable boot-up from it.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos