RT1060 SDK 提供的wifi例程是基于什么wifi芯片?博通?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1060 SDK 提供的wifi例程是基于什么wifi芯片?博通?

1,125 Views
2291127076
Contributor I

你好:

        我现在在rt板子上调sdk中的wifi例程。我选用的wifi芯片是博通的43436B0,我移植了43436B0的驱动到sdk中。

但是出现了一下的log:

Initializing WiFi connection... 
Could not initialize bus
Could not initialize wifi platform
Could not initialize WiFi module 2
No connectivity.

下面我想存在一些问题,想要咨询你们:

1.关于wifi sdio接口的问题,在sdk iperf_wifi例程中,配置了以下引脚。pastedImage_1.png

在博通wifi中,除了以上引脚,还有额外的引脚,比如下图的WL_REG_ON和WL_HOST_WAKE,这个对调试wifi有影响吗? 针对这个一下这个芯片,除了正常工作之外,SDIO接口应该怎么和rt开发板保持一致,你们能给个方案吗?

pastedImage_3.png

2.RT1060 SDK 提供的wifi例程是基于什么wifi芯片?博通?

3.我们想在rt板子上支持博通wifi,同时支持ble,你们有推荐吗?此外,在移植wifi过程中的重要点,你能答复我一下吗?

Tags (2)
0 Kudos
1 Reply

1,043 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi zhao yang ,

1.关于wifi sdio接口的问题

 答:

WL_REG_ON和WL_HOST_WAKE,我觉得这个问题你可以问问博通那边,这个芯片的控制对wifi的具体影响。

需要给什么信号,然后RT给出对应的信号即可。

关于SDIO, 你可以直接参考SDK的对应代码。

- Murata 1DX M.2 module
- Murata uSD M.2 Adapter

这个是murata的模块,然后具体芯片是

2.RT1060 SDK 提供的wifi例程是基于什么wifi芯片?博通?

 答:在SDK的wifi例程中,你可以发现:

- Murata 1DX M.2 module
- Murata uSD M.2 Adapter

https://wireless.murata.com/usd-m2.html

https://wireless.murata.com/type-1dx.html

https://www.embeddedartists.com/products/1dx-m-2-module/

模块是murata的,里面的wifi芯片是crypress的

pastedImage_1.png

3.我们想在rt板子上支持博通wifi,同时支持ble,你们有推荐吗?此外,在移植wifi过程中的重要点,你能答复我一下吗?

 答: 我们现在RT SDK所支持的wifi模块就可以同时支持BLE, 关于博通的情况,还请咨询博通那边。

Wish it helps you!

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos