RT105x FlexRAM configuration using the DCD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT105x FlexRAM configuration using the DCD

874 Views
gaetano81
Contributor I

Hello Yuri,

is it possible to set  IOMUXC_GPR_GPR17 and IOMUXC_GPR_GPR16 using Device Configuration Data?

 

Regards 

Gaetano

Labels (1)
0 Kudos
1 Reply

657 Views
Yuri
NXP Employee
NXP Employee

Hello,

   i.MX RT1050 Reference Manual (Rev. 1, 03/2018) mentions the list of allowable
blocks and target addresses for the chip, which may be written, using the DCD,

but the list is skipped. Generally IOMUX_GPR area should be included in the valid

DCD ranges; in any case customers  can also use a plugin image running in OCRAM.  


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos