RT1052 using DMA to modify the PWM duty cycle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1052 using DMA to modify the PWM duty cycle

971 Views
617906872
Contributor I

Does anyone have an example of RT1052 using DMA to modify the PWM duty cycle? Can you send me a copy? My email: 617906872@qq.com, thank you very much

Labels (1)
0 Kudos
3 Replies

841 Views
617906872
Contributor I

I have already seen that example, thank you very much, it can be used and meet the requirements. I don't know now that eFlexPWM and QTimer are the same peripheral? QTimer can realize PWM output. Is eFlexPWM also dependent on QTimer?

0 Kudos

841 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

 

No, they are no dependent.

 

Regards,

Felipe

0 Kudos

841 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello,

 

There is an example on our official SDK that implements QTMR driver's input capture and output pwm feature by DMA. Maybe it can be helpful for you.

 

You can download SDK from the below link.

Welcome | MCUXpresso SDK Builder 

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------