RT1052 SEGGER RTT not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1052 SEGGER RTT not work

1,059件の閲覧回数
wandongli
Contributor I

I ported SEGGER RTT to RT1052, but he can't run, there is nothing to output, help me.

ラベル(1)
0 件の賞賛
1 返信

864件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,
RTT is provided by Segger, and there are not additional specific information/guidelines for using it on i.MX RT. So, in this case, you should directly contact Segger for support.
As complementary information, you could take a look at the following link:

https://mcuoneclipse.com/2015/07/07/using-segger-real-time-terminal-rtt-with-eclipse/


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛