RT1052 SEGGER RTT not work

cancel
Showing results for 
Search instead for 
Did you mean: 

RT1052 SEGGER RTT not work

756 Views
wandongli
Contributor I

I ported SEGGER RTT to RT1052, but he can't run, there is nothing to output, help me.

Labels (1)
0 Kudos
1 Reply

561 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,
RTT is provided by Segger, and there are not additional specific information/guidelines for using it on i.MX RT. So, in this case, you should directly contact Segger for support.
As complementary information, you could take a look at the following link:

https://mcuoneclipse.com/2015/07/07/using-segger-real-time-terminal-rtt-with-eclipse/


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos