RT1052 DTCM 非对齐访问引起的hardfault问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1052 DTCM 非对齐访问引起的hardfault问题

3,666 Views
1099789860
Contributor II

现象是:在启动文件中使用FlexRAM重新分配RAM给DTCM(448K),发现在前128K内访问内存不用对齐,而128K之后访问内存必须对齐否则将引起非对齐访问错误HardFAUlt,想问为什么128K内可以不对齐而128K之后则需要对齐?该测试是在启动文件里重新分配的RAM,分散加载使用的数据区域是0x20000000~0x00070000,具体测试情况如下。

1.发现当使用超过128K地址(0x20000000~0x20020000)之后的RAMmemcpy必须四字节对齐,直接按short类型访问则必须2字节对齐,直接按int类型访问必须4字节对齐,否则引起非对齐访问错误HardFault

2.128K地址(0x20000000~0x20020000)内的空间,分别进行上述3种操作,不对齐时仍正常。

3.看(https://community.nxp.com/thread/487135)的评论NXP提供的两个重新分配代码,我使用后发现并没有解决这个问题。请问该如何解决?

4.我的代码如下:

unsigned char testtr[10] __attribute__((at(0x20020001)));

void HardFault_Handler() {

   PRINTF("Hard_FaulT\r\n");

   if(SCB->CFSR & (1<<24)) PRINTF("   非对齐访问错误(UNALIGNED)!\r\n");

   while(1);

}

main函数内的测试代码:

   memcpy(testtr,"0123456789",10); /* 超过128k后 必须四字节对齐,否则引起非对齐访问错误 */

   testtr[0] = 0x3;

   PRINTF("单字节访问成功\r\n");

   

   *((uint16_t *)testtr) = 0xff;/* 超过128k后,双字节访问时必须2字节对齐,否则引起非对齐访问错误 */

   PRINTF("双字节访问成功\r\n");

   

   *((uint32_t *)testtr) = 0xff;/* 超过128k后,四字节访问时必须4字节对齐,否则引起非对齐访问错误 */

   PRINTF("四字节访问成功\r\n");

启动文件测试代码有三个,测试结果是一样的。

;测试代码1:512KB全分配给DTCM 配置结果是GPR14 = 0x00A00000 GPR16 =0x00200006 GPR17 = 0xAAAAAAAA
                LDR     R0, =0x400AC038
                LDR     R1, =0x00A00000
                STR     R1, [R0]
                
                LDR     R0, =0x400AC040
                LDR     R1, =0x00200006
                STR     R1, [R0]
               
                LDR     R0, =0x400ac044 
                LDR     R1, =0xAAAAAAAA 
                STR     R1, [R0]


;测试代码2,来自于NXP社区:512KB全分配给DTCM.配置结果是GPR16 =0x00200007 GPR17 = 0xAAAAAAAA
;        LDR     R0, =0x400ac044
;        LDR     R1, =0xaaaaaaaa
;        STR     R1,[R0]
;        LDR     R0,=0x400ac040
;        LDR     R1,=0x04
;        LDR     R3,[R0]
;        ORR     R2,R1,R3
;        STR     R2,[R0]


;测试代码3,来自于NXP社区:DTCM是448K OCRAM是64K
;                LDR     R0, =OCRAM_Reallocate
;                BLX     R0
;                LDR     R0, =0x400B0000
;                LDR     R2, =FLEXRAM_Init
;                BLX     R2

Labels (1)
0 Kudos
4 Replies

3,341 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 永超 赵 ,

非常感谢使用NXP产品,很高兴为你提供技术支持!
请分享你的测试代码,我这边复现确认一下并查找其原因。
期待你的回复。

Have a great day,
TIC

 

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

3,341 Views
1099789860
Contributor II

谢谢,进一步分析得到的结论:128k之后(0x20020000之后)的空间,使用STRH指令访问必须2字节对齐(C语言中按short类型访问),使用STR指令访问必须4字节对齐(C语言中按int类型访问),否则将引起UNALIGNED HardFault。而0x20000000~0x20020000内的空间,STRH指令与STR指令无限制,不会引起hardFault。而memcpy会调用STR指令,所以memcpy要求四字节对齐。

代码路径:\SDK_2.4.1_EasyARM-RT1052-V1_0_2018-12-27\boards\EasyARM-RT1052-V1_0\demo_apps\hello_world 0.1      《hello_world flexspi_nor_debug标签

0 Kudos

3,341 Views
1099789860
Contributor II

您好,这个问题已经解决了,很感谢您的支持。详情见https://community.nxp.com/thread/487135,大致概括一下原因:FlexRAM的配置之后未相应改变MPU的设置。

3,341 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 永超 赵 ,

感谢回复,很高兴听到问题解决。

Have a great day,
TIC

 

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos