RT1050 with external 16-bit low power SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1050 with external 16-bit low power SDRAM

780 次查看
matthiaspimming
Contributor I

I have configured the RT1050 to use the SEMC to interface to a external 16-bit SDRAM. The SDRAM is a Winbond 512Mb Low Power SDRAM (W989D6DB) operating at 1.8V power supply.

The SDRAM works fine most at the time, but some times it happens that the memory access fails after power up sequence. Does any one have a idea what can cause this problem?

标签 (1)
标记 (3)
0 项奖励
1 回复

593 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   I think, it makes sense to discuss memory (power up) initialization sequence

with memory manufacturer directly. I do not see such specs in their Datasheet.

https://www.winbond.com/resource-files/w989dxdb_pkg_datasheet_a01-002_20161201.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励