RT1050 with external 16-bit low power SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050 with external 16-bit low power SDRAM

772 Views
matthiaspimming
Contributor I

I have configured the RT1050 to use the SEMC to interface to a external 16-bit SDRAM. The SDRAM is a Winbond 512Mb Low Power SDRAM (W989D6DB) operating at 1.8V power supply.

The SDRAM works fine most at the time, but some times it happens that the memory access fails after power up sequence. Does any one have a idea what can cause this problem?

Labels (1)
0 Kudos
1 Reply

585 Views
Yuri
NXP Employee
NXP Employee

Hello,

   I think, it makes sense to discuss memory (power up) initialization sequence

with memory manufacturer directly. I do not see such specs in their Datasheet.

https://www.winbond.com/resource-files/w989dxdb_pkg_datasheet_a01-002_20161201.pdf 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos