RT1050: using BEE address remapping to swap FW in XIP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050: using BEE address remapping to swap FW in XIP

Jump to solution
876 Views
leopoldgemsch
Contributor I

Dear all,

we are analyzing how it would be possible to swap between different application FW in a FlexSPI NOR FLASH to be executed without need of relinking/downloading the binaries.

The .MX RT105x has a BEE which supports two address areas to be mapped. Does someone know, can this feature being used to remap a memory area within the FlexSPI AHB bus space to swap between two different application FW executed in XIP mode?

For any response many thanks

Labels (1)
0 Kudos
1 Solution
836 Views
FelipeGarcia
NXP Employee
NXP Employee

We do not have an example of this but you can find more information about this feature in the BEE chapter of the Secure Reference Manual.

Regards,

Felipe

View solution in original post

0 Kudos
3 Replies
867 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Flash remapping feature is only available with RT106x devices. You can find more information about this in the following application notes.

https://www.nxp.com/docs/en/application-note/AN12240.pdf

https://www.nxp.com/docs/en/application-note/AN12255.pdf

For RT1050, it don't support flash remap same as RT1060, but BEE can do similar function, so if you enable BEE in your application, you can implement image remapping by BEE offset.

Best regards,

Felipe

0 Kudos
854 Views
leopoldgemsch
Contributor I

Dear Felipe,

many thanks for this hint.
- Is it possible to use the remapping of BEE without having the FW image encrypted?
- Is there an example existing, how this would work?

Many thanks for a replay

0 Kudos
837 Views
FelipeGarcia
NXP Employee
NXP Employee

We do not have an example of this but you can find more information about this feature in the BEE chapter of the Secure Reference Manual.

Regards,

Felipe

0 Kudos