RT1050-EVKB: SW5 DIP not fitted (SW5-1 is EncryptXIP)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1050-EVKB: SW5 DIP not fitted (SW5-1 is EncryptXIP)

804 次查看
rshipman
Contributor V

Why are the DIP switches SW5 and SW6 not fitted to the RT1050-EVKB eval board?

Especially SW5, because SW5-1 is used to enable Encrypt XIP.

It is a bit annoying having to solder on our own...

Note that the RT1020-EVK has a single SW8 DIP, where SW8-1 is the switch to enable Encrypt XIP.

So I'm wondering why SW5 was not provided for the RT1050-EVKB?

标签 (2)
0 项奖励
1 回复

749 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Ronnie,

 

I am sorry for my late reply. You are correct, SW5 and SW6 are not populated in the board so customers can decide to included or not. These are design internal decisions.

 

Sorry for the inconveniences this may have caused you.

 

Best regards,

Felipe

0 项奖励