RT101X USB FS/HS device without external crystal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT101X USB FS/HS device without external crystal

跳至解决方案
502 次查看
jh0
Contributor IV

Does RT101X can work as FS or / and HS USB device (not host) without using external crystal?

Regards,

JH

0 项奖励
1 解答
496 次查看
jay_heng
NXP Employee
NXP Employee

External 24MHz crystal is necessary for USB application (PHY should be driven by 480MHz clk). as internal RC24M (maximum 20% accuracy error) is only for low speed peripherals

在原帖中查看解决方案

1 回复
497 次查看
jay_heng
NXP Employee
NXP Employee

External 24MHz crystal is necessary for USB application (PHY should be driven by 480MHz clk). as internal RC24M (maximum 20% accuracy error) is only for low speed peripherals