Hi
I am testing an application. (SDK: evkmimxrt1015_iled_blinky)
I expect this application can execute from sdphost in download mode.
I think it's possible.
My Step are:
1. make RT1015 to download mode
2. Load my test application to 0x20208000
3. jump to 0x20208000.
The result is fail, the led is not blinking.
Can anyone teach me how to modify the evkmimxrt1015_iled_blinky so that it can run in sdphost jump?
Thanks
Ken
Solved! Go to Solution.
Hi kensu,
感谢你的信息更新!
你可以试想下flashloader.bin是什么?
它其实就是一个特殊应用app对不对,然后是放到RAM,并且跳转过去运行的,所以如果你的app本身就是RAM的,我认为你完全可以这么干,你可以试试,如果有问题,我们再继续交流。
你可以模仿flashloader那样去做。
Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hi kensu,
Can you read the chinese document?
If yes, please read these post, it will be useful to you:
https://www.cnblogs.com/henjay724/p/9096222.html
https://www.cnblogs.com/henjay724/p/11992494.html
This is my post about how to use the sdphost and the blhost to download the ledblinky code for RT1064:
http://www.nxpic.org.cn/module/forum/thread-620980-1-1.html
RT1015 is similar.
Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hi Kerry
谢谢回覆
但我这边要试的是并不是SDPHOST + BLHOST将application烧到Flash内
我想试的是: 将application透过SDPHOST放在SRAM内,然后Jump直接执行这个Application
标准方式:
1. SDPHOST将FlashLoader.bin放到SRAM
2. SDPHOST Jump到SRAM的位置开始执行FlashLoader
3. BLHOST下command给SRAM的FlashLoader,将application烧录到Flash
4. DIP Switch改成boot mode执行application
而我想试的是
1. SDPHOST直接将Application.bin放到SRAM
2. SDPHOST Jump到SRAM的位置开始执行Application
有机会吗?
Regards
Ken
Hi kensu,
感谢你的信息更新!
你可以试想下flashloader.bin是什么?
它其实就是一个特殊应用app对不对,然后是放到RAM,并且跳转过去运行的,所以如果你的app本身就是RAM的,我认为你完全可以这么干,你可以试试,如果有问题,我们再继续交流。
你可以模仿flashloader那样去做。
Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------