RT 1020 A/B system updates

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT 1020 A/B system updates

Jump to solution
942 Views
dmondou
Contributor I

Is there a boot loader for the RT 1020 that can handle an A/B update strategy for field updates? For example:
The device would be configured with an active and inactive partition for holding firmware. Partition A would be programmed with firmware at the factory and partition B would be empty. After receiving an updated image over Ethernet the updated image would be written to partition B. Partition A would be deactivated and partition B would be activated. On reset the boot loader would then load the image from partition B, if the image failed to run on reset the boot loader would then fail over to running partition A. If successful it would continue to boot from partition B until the next update. That update would then be written to slot A and the process would repeat.

0 Kudos
1 Solution
829 Views
jeremyzhou
NXP Employee
NXP Employee

Hi David Mondou,

To be honest, this bootloader scheme you proposed is a bit complicated.
And there's no similar application note for you to refer to now.
It needs the customers to develop by themselves.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
830 Views
jeremyzhou
NXP Employee
NXP Employee

Hi David Mondou,

To be honest, this bootloader scheme you proposed is a bit complicated.
And there's no similar application note for you to refer to now.
It needs the customers to develop by themselves.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos