Question about RMII connection on RT1050EVKB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about RMII connection on RT1050EVKB

1,087 Views
giuseppescarpi
Contributor III

I am studying the schematic of the new (A1) version of the RT1050 EVK board.

The schematic shows the signal ENET_CRS_DV coming from the PHY to MCU pin C12, which is described as "ENET_RX_EN". On the other hand, signal ENET_INT goes to G13, which can be associated to ENET_CRS.

So I wonder if these two signals are swapped, or if there is something I am missing (quite possible, I'm not an expert of Ethernet).

Hints and suggestions?

Giuseppe

Labels (1)
0 Kudos
2 Replies

14 Views
Johnrita
Contributor I

Hi, I was curious why does the Pin CRS_DV only selected on G13 but not C12, while EVB sch shows it located on C12?

Does it correct?

0 Kudos

914 Views
igorpadykov
NXP Employee
NXP Employee

Hi Giuseppe

for names of rmii signals and its usage may be useful also to look

How to use i.MX6SDL ENET_CRS_DV pad for CRS for RMII mode. 

I think there is no swapping, ENET_INT is handled processor as gpio interrupt.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos