Query related to Power consumption is DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Query related to Power consumption is DMA

ソリューションへジャンプ
990件の閲覧回数
suhel_mulla
Contributor III

Hello,

We are using NXP i.MX RT 1052 controller.

We already know that DMA is used for parallel processing and to improve overall processor performance.

But, we are trying to understand whether DMA can be used to minimize current consumption or not.

My question is as below -

Consider the below 2 cases,

  1. SPI DMA is used to transfer SPI data between memory and SPI transfer registers, CPU(Cortex M7 core) is in sleep mode.
  2. Normal SPI is used (SPI DMA is not enabled) to transfer the same amount of data between memory and SPI transfer registers using CPU.

For these 2 cases, in which case, the current consumption will be more?

Also, please provide if any analytical document is available for this.

ラベル(1)
タグ(5)
0 件の賞賛
1 解決策
985件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) My question is as below -
Consider the below 2 cases,
SPI DMA is used to transfer SPI data between memory and SPI transfer registers, CPU(Cortex M7 core) is in sleep mode.
Normal SPI is used (SPI DMA is not enabled) to transfer the same amount of data between memory and SPI transfer registers using the CPU.
For these 2 cases, in which case, the current consumption will be more?
-- Case 2 will cost more power consumption.
And there's an article that explains the DMA's advantage and hopes it can help you.

Hope it helps.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
980件の閲覧回数
suhel_mulla
Contributor III

Thanks for the answer and sharing the article. It will solve my query.

0 件の賞賛
984件の閲覧回数
suhel_mulla
Contributor III

Thanks for the answer.

Can you share link of the article which explains it?

0 件の賞賛
986件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) My question is as below -
Consider the below 2 cases,
SPI DMA is used to transfer SPI data between memory and SPI transfer registers, CPU(Cortex M7 core) is in sleep mode.
Normal SPI is used (SPI DMA is not enabled) to transfer the same amount of data between memory and SPI transfer registers using the CPU.
For these 2 cases, in which case, the current consumption will be more?
-- Case 2 will cost more power consumption.
And there's an article that explains the DMA's advantage and hopes it can help you.

Hope it helps.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛