Power Group Conflict

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power Group Conflict

955 Views
sumant_s_khalat
Contributor II

Hi,

I'm interfacing an eMMC chip to the i.MXRT1062 controller using USDHC2 peripheral. For the eMMC to support HS200 mode the VDDQ Voltage(I/O Voltage) of eMMC need to be between 1.7V–1.95V i.e 1.8V.

I can change the NVCC_SD1 voltage to 1.8V and can get away with it, but it looks like the CSX,1 pin from SEMC also uses this voltage group(The rest of SEMC pins uses 3.3V).

There is no other option available for me to change the MUXing of CSX,1 or use any other CSX as all other pins have been consumed.

pastedImage_1.png

So my questions are,

1. Why isn't the tool generating a warning when the SEMC is using 2 different voltages?

2. Is there any way out? apart from using a hardware voltage level converter at CSX,1 to make it 3.3V compatible

Regards,

Sumant

Labels (1)
Tags (2)
0 Kudos
3 Replies

839 Views
sumant_s_khalat
Contributor II

Hi YuriMuhin_ng,

Thanks for your reply.

First things first, I have already configured the power groups as bellow.

pastedImage_1.png

Secondly, all the pins from SEMC peripheral (apart from CSX,1) use NVCC_EMC power rail which is at 3V3.

Now for CSX,1 I have 2 options as you said:

   1. Use L4 pin, GPIO_SD_B1_07, powered by NVCC_SD1
   2. Use D7 pin, GPIO_B0_00, powered by NVCC_GPIO

But I can't go with either option as pin L4 which is using NVCC_SD1 power rail is at 1V8 and pin D7(NVCC_GPIO-3v3) is already been used for ENET2_MDC and I can't change the muxing of ENET2_MDC as the other optional pin is already used for another purpose.

 

So the question remains,

1. Even after having the power group defined, why didn't the tool generated a power group conflict warning?

pastedImage_6.png

2. Can we stick to the same pin(L4, NVCC_SD1-1V8) and use an external hardware voltage level conversion circuit to switch the 1V8 signal to 3V3 as the CSX, 1 is only output signal? and how common is this approach? do you see any downside of it or foresee any problem?

Regards,

Sumant 

0 Kudos

839 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   The SEMC_CSX,1 as  GPIO_SD_B1_07 is powered by NVCC_SD1 - that is,

the same voltage is used as for the rest uSDHC2 signals (SD_B1 group), therefore

there is no voltage conflict here. Generally it is possible to use voltage convertor for

the output SEMC_CSX,1 signal.

Regards,

Yuri.

0 Kudos

839 Views
Yuri
NXP Employee
NXP Employee

Hello,

   It is possible to use different pin mux-ing options for the pins in order to avoid

conflicts. For example SEMC CSX1 has two options:

  L4 pin, GPIO_SD_B1_07, powered by NVCC_SD1

  and
  D7 pin, GPIO_B0_00, powered by NVCC_GPIO

Note, in order to get warnings regarding power voltages conflicts - it is needed to

setup power supply voltages (in Power Groups tab of the i.MX Pins tool).

Pins Tool for i.MX Application Processors | NXP 

Have a great day,
Yuri

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos