PE Micro with IMXRT1020 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PE Micro with IMXRT1020 EVK

768 Views
narenchandra401
Contributor III

Hi community people

We are using IMXRT1020 EVK board , We want to test flashing with PE Micro Universal , Can some one guide on the board settings 

We have IMXRT1020 EVK , PE Micro Universal JTAG 

Connected the JTAG 20 pin connector to J16 of the board , 

Checked that jumpers J27 and J28 are off (they are on by default when boards ship from the factory) to ensure SWD signals are disconnected from the OpenSDA microcontroller.

In the IDE we have selected PE Micro in Debug configuration 

79039070.PNG

We are facing the below error , Please suggest the proper settings 

DC844D6B.PNG

Labels (1)
Tags (3)
2 Replies

651 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Naren,

Yes, you can disconnect J27 and J28, then connect Multilink Universal to J16. That should be enough.

https://community.nxp.com/message/1044022?commentID=1044022#comment-1044022 

Maybe you can try to update Multilink firmware. 

http://www.pemicro.com/downloads/download_file.cfm?download_id=346 

Here is other people who ask similar question.

https://community.nxp.com/message/1163806?commentID=1163806#comment-1163806 

Regards,

Jing

651 Views
narenchandra401
Contributor III

Thanks Jing Pan ,

That was helpful 

0 Kudos