Oscillator tolerance of mimxrt1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Oscillator tolerance of mimxrt1064

565 Views
chenfei_203
Contributor I

Hello community,

 

I hope to know a 24 MHz oscillator tolerance of mimxrt1064 in consideration of USB

 

Best regards.

Labels (2)
0 Kudos
1 Reply

506 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello,

 

The peripheral clock tolerance requirements are really coming from end use and compatibility with other devices rather than being a requirement from the RT10xx itself. The tolerances showed below are based on the standard specifications for the protocols listed so you could take them as reference.

pastedImage_2.png

I hope it helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------