Offline tool that converts SVG to Elementary structures

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Offline tool that converts SVG to Elementary structures

Jump to solution
1,199 Views
AndyCapon
Contributor II

Hi Guys,

I'm looking for the tool mentioned in AN13075:

Note: The map is rendered using a rendering library called “Elementary”. This library uses VGLite to render vector objects and bitmaps. It is divided into two parts: an offline tool that converts SVG to Elementary structures and a runtime that interprets those structures into VGLite-usable code. The runtime source code is provided with the i.MXRT1170 SDK. For the offline tool, contact the NXP community.

The included VGLite examples in the SDK also use this "Elementary" library.

Does anyone have any idea where I can get this from?

All the best

Andy

0 Kudos
1 Solution
1,169 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Sorry for the reply late and I receive the reply from the AE team currently.
They say the tool will need to wait a while to release.
So please wait a while more patiently for the official software to be released.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
4 Replies
1,192 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I've not found any further information about ''the offline tool'' in the NXP website and I guess it's not released, I'll contact the AE for confirmation.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
1,189 Views
AndyCapon
Contributor II

Hi Jeremy,

Thanks very much for looking into this for me.

Cheers

Andy

0 Kudos
1,170 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Sorry for the reply late and I receive the reply from the AE team currently.
They say the tool will need to wait a while to release.
So please wait a while more patiently for the official software to be released.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,160 Views
AndyCapon
Contributor II

Hi Jeremy,

Thanks very much for the feedback, I will keep an eye out.

Cheers

Andy

0 Kudos