Nor flash map for i.MXRT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nor flash map for i.MXRT1170

582 Views
jimmyli
Contributor IV

Hi,

     Why m_flash_config_start must start at 0x30000400, while 0x30000000 will be failed?

     Note: For i.MXRT1060, 0x60000000 is OK.

     Thanks.

jimmyli_0-1640574133889.png

 

0 Kudos
2 Replies

577 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Why m_flash_config_start must start at 0x30000400, while 0x30000000 will be failed?
-- Just as the below figure shows, the ROM code will fetch the 512-byte FlexSPI NOR configuration parameters start from the offset 0x400 in Serial NOR flash attached to FLEXSPI_A_SS0_B during the boot-up process.

jeremyzhou_0-1640584721299.png

I think it can explain your question, however for the RT1060/50, FlexSPI NOR configuration parameters should be resided at the beginning address of Serial NOR flash.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

567 Views
jimmyli
Contributor IV

Hi TIC,

      It is great for me by this reply.

      Thanks.

0 Kudos