NCache Region Overflow Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NCache Region Overflow Error

Jump to solution
1,924 Views
omerkaanbasakin
Contributor IV

Hı ı am working on imxrt 1052 with custom board. Using Mcuxpresso 11.1.1 and SDK_2.7.0_MIMXRT1052xxxxB . I encountered an error during debug session and ı can not understand what the problem is . I tried to optimize (properties -> setings ->MCU C compiler -> optimization -> optimization level -> optimize for size , optimize for debug (ı tried both))  but error messages not change, only the numberof bytes changed. 

void BOARD_ConfigMPU(void)
{
#if defined(__CC_ARM) || defined(__ARMCC_VERSION)
extern uint32_t Image$$RW_m_ncache$$Base[];
/* RW_m_ncache_unused is a auxiliary region which is used to get the whole size of noncache section */
extern uint32_t Image$$RW_m_ncache_unused$$Base[];
extern uint32_t Image$$RW_m_ncache_unused$$ZI$$Limit[];
uint32_t nonCacheStart = (uint32_t)Image$$RW_m_ncache$$Base;
uint32_t size = ((uint32_t)Image$$RW_m_ncache_unused$$Base == nonCacheStart) ?
0 :
((uint32_t)Image$$RW_m_ncache_unused$$ZI$$Limit - nonCacheStart);
#elif defined(__MCUXPRESSO)
extern uint32_t __base_NCACHE_REGION;
extern uint32_t __top_NCACHE_REGION;
uint32_t nonCacheStart = (uint32_t)(&__base_NCACHE_REGION);
uint32_t size = (uint32_t)(&__top_NCACHE_REGION) - nonCacheStart;
#elif defined(__ICCARM__) || defined(__GNUC__)
extern uint32_t __NCACHE_REGION_START[];
extern uint32_t __NCACHE_REGION_SIZE[];
uint32_t nonCacheStart = (uint32_t)__NCACHE_REGION_START;
uint32_t size = (uint32_t)__NCACHE_REGION_SIZE;
#endif
uint32_t i = 0;

/* Disable I cache and D cache */
if (SCB_CCR_IC_Msk == (SCB_CCR_IC_Msk & SCB->CCR))
{
SCB_DisableICache();
}
if (SCB_CCR_DC_Msk == (SCB_CCR_DC_Msk & SCB->CCR))
{
SCB_DisableDCache();
}

/* Disable MPU */
ARM_MPU_Disable();

/* Region 0 setting: Memory with Device type, not shareable, non-cacheable. */
MPU->RBAR = ARM_MPU_RBAR(0, 0x80000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_512MB);

/* Region 1 setting: Memory with Device type, not shareable, non-cacheable. */
MPU->RBAR = ARM_MPU_RBAR(1, 0x60000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_512MB);

#if defined(XIP_EXTERNAL_FLASH) && (XIP_EXTERNAL_FLASH == 1)
/* Region 2 setting: Memory with Normal type, not shareable, outer/inner write back. */
MPU->RBAR = ARM_MPU_RBAR(2, 0x60000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_RO, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_64MB);
#endif

/* Region 3 setting: Memory with Device type, not shareable, non-cacheable. */
MPU->RBAR = ARM_MPU_RBAR(3, 0x00000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_1GB);

/* Region 4 setting: Memory with Normal type, not shareable, outer/inner write back */
MPU->RBAR = ARM_MPU_RBAR(4, 0x00000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_128KB);

/* Region 5 setting: Memory with Normal type, not shareable, outer/inner write back */
MPU->RBAR = ARM_MPU_RBAR(5, 0x20000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_128KB);

/* Region 6 setting: Memory with Normal type, not shareable, outer/inner write back */
MPU->RBAR = ARM_MPU_RBAR(6, 0x20200000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_256KB);

/* Region 7 setting: Memory with Normal type, not shareable, outer/inner write back */
MPU->RBAR = ARM_MPU_RBAR(7, 0x80000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_32MB);

while ((size >> i) > 0x1U)
{
i++;
}

if (i != 0)
{
/* The MPU region size should be 2^N, 5<=N<=32, region base should be multiples of size. */
assert(!(nonCacheStart % size));
assert(size == (uint32_t)(1 << i));
assert(i >= 5);

/* Region 8 setting: Memory with Normal type, not shareable, non-cacheable */
MPU->RBAR = ARM_MPU_RBAR(8, nonCacheStart);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 1, 0, 0, 0, 0, i - 1);
}

/* Enable MPU */
ARM_MPU_Enable(MPU_CTRL_PRIVDEFENA_Msk);

/* Enable I cache and D cache */
SCB_EnableDCache();
SCB_EnableICache();
}

pastedImage_5.png

pastedImage_6.png

pastedImage_7.png

Labels (1)
0 Kudos
1 Solution
1,809 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Omer,

It seems you put to much things in NCACHE_REGION. This region is at the end of SDRAM. You can enlarge its size.

Regards,

Jing

View solution in original post

0 Kudos
2 Replies
1,810 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Omer,

It seems you put to much things in NCACHE_REGION. This region is at the end of SDRAM. You can enlarge its size.

Regards,

Jing

0 Kudos
1,809 Views
omerkaanbasakin
Contributor IV

Hi jingpan‌,

Thanks for your reply. 

It seems solved the probelm

0 Kudos