My Application is not able to detect SD Card from i.MX RT595 Evaluation Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

My Application is not able to detect SD Card from i.MX RT595 Evaluation Kit

373 Views
Charan0705
Contributor I

We have copied PCM files in SD Card and inserted SD Card into RT595 D1 board.
When our Application tries to open the PCM file from SD Card, it strucks at line no. 733 in fsl_usdhc.c file.

0 Kudos
3 Replies

345 Views
Charan0705
Contributor I

Hi @EdwinHz ,

Please find the attached image of the RT595 module what we are using.
And upon this, our own custom application is running, in which we are facing this issue.
Can we have a call, so that you will get more details of this issue, in which we can get more info from you as well to make this issue into resolve state.

Thanks
Charan 

0 Kudos

326 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi again @Charan0705,

Considering that you are using the EVK, please do try our SDK example codes to ensure that the SD Card module is working properly. Since the demo codes are created specifically to work for our EVKs, successfully running the example will discern whether the issue is coming from your custom SW, or from the EVK's hardware.

BR,
Edwin.

0 Kudos

363 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Charan0705,

Are you using a custom board or our EVK? Please try using our SDK example codes to ensure that the HW connection is adequate. 

BR,
Edwin

0 Kudos